After grinding in the ball mill, fragments of ore remain that are too large to pass through the screen to the next phase. These fragments, along with foreign matter that can include broken balls from the mill, are ushered to the rejects line. Valves isolating these lines must provide zero leakage shutoff to prevent valuable water loss, while also being robust enough to resist severe impact damage.
Optimize Your Process With Genuine Knife Gate Valve Parts, Ensuring Safety & Productivity
The following products are capable of providing zero leakage shutoff of ball mill reject lines. They are also engineered to resist heavy impact damage and extend the uptime of your mill.
Andy Coxall joins podcast host Jim Cahill to discuss the challenges in tailings management, the problems with valves not suited for this severe-service application, and why severe-service knife gate valve technology such as the Clarkson KS1 is the best choice for these challenging slurry applications.
read moreBased on many plant visits and discussions with Emerson customers, I have concluded that handling slurries is one of the biggest problems for operators and reliability teams. The most frequently mentioned issues are clogging and erosion, which certainly take their toll, but there is also a more subtle challenge related to measuring flow. Why slurries …
read moreEn este episodio los expertos en instrumentación industrial, Jorge Espinoza y Martín López nos comparten sobre las tecnologías de medición y monitoreo para variables críticas en la industria minera. Exponen sobre los más recientes avances en medición para incrementar la seguridad, la eficiencia y la rentabilidad de los procesos mineros. Te invitamos a ver o …
read more